This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
A microcontroller was developed in 1971 by Intel Corporation in the United States.
That is the 4 bit microcontroller called i4004.
It was ordered by a Japanese company BUSICOM for calculators.
Later, the contract was changed and it was sold as a general-purpose microcontroller with success.
After that, Intel Corp. developed a 16 bit microcontroller ‘8086,’ following the 8 bit microcontrollers such as ‘i8008’, ‘i8080A,’ and ‘i8085.’
After developing several microcontrollers, they continue to develop the CPUs used in current personal computers.
Toshiba developed a 12 bit microcontroller TLCS-12 in 1973.
At that time, the United States was considering electronic control units as a countermeasure of the exhaust gas regulation law.
Against this background, Toshiba's 12 bit microcontroller was developed as Ford's in-vehicle engine controller.
After that, Toshiba developed a wide range of high-level microcontrollers from 4 bit to 32 bit or higher.