This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
There are three types of bus lines: Data bus, Address bus, and Control bus.
Communication over each bus line is performed in cooperation with another.
The data bus is a signal line for exchanging the data between the CPU and the memory, and between the CPU and I/O, and handles the data stored in the specified location.
The data exchanged includes numerical values for calculation, the calculation results, input signals from external devices, and signals output to external devices.
The address bus is a signal line that specifies the location of the memory and I/O.
When exchanging data, it is necessary to specify the takeoff-destination of the data or the storage destination of the data.
The address bus specifies this location.
The control bus is a signal line that specifies whether to read or write to the location specified by the address bus.
The memory and I/O specified on the address bus receive the data which sent on the data bus when instructed "Write" by the control bus.
When instructed "Read" by the control bus, the data is output to the data bus.