This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
The figure on the right shows the hardware configuration of a microcontroller.
First of the five elements, the CPU that takes charge of calculation and control will be explained later.
The CPU is generally called the "center of the microcontroller" or the "brain of the microcontroller".
CPU is an abbreviation that combines C of "Central", P of "Processing", and U of "Unit".
It can be said that the CPU is located in the center of the microcontroller and is the part for processing.
“Processing" can mean adding or subtracting data.
For this reason, the CPU is called the central processing unit