This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Let's look at the stator's magnetic poles and the rotor movement with the 2-phase 4-pole motor as shown below when the current direction of the stator winding is repeatedly switched.
The rotor makes a step operation by switching the current direction in the winding of the stator, the magnetic poles of the rotor and the magnetic poles of each phase of the stator repelling and attracting.
Therefore, the stepping motor rotates when the above is performed continuously.