This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
SPST and SPDT are abbreviation commonly used to describe switches. SPST is an abbreviation for Single-Pole Single-Throw, and Pole refers to the number of circuits that one switch can control "simultaneously". Throw also represents the number of outputs that can be switched.
For example, SPDT is SP (Single pole) because one switch can control one circuit at a time, and DT (Double throw) because it can switch two outputs. (Table-1)
Table-1 Function name of Bus switches
The following documents also contain related information.