This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
In most cases, putting a product with a Schmidt trigger function on the input will solve the problem. Products without a Schmitt trigger function on the input may experience chattering due to low slew rate signals.
Schmitt trigger function has a hysteresis voltage VH between the input High level threshold voltage VP and Low level threshold voltage VN. Therefore, even if noise enters the signal when the input transitions from Low to High, it will not become High unless the voltage of VP is exceeded. In addition, once it becomes High, it will remain High even if the voltage drops slightly, unless it drops below VN. In this way, chattering, which is a problem with signals with a low slew rate (also known as signal slow input when the input rise/fall time is slow), is less likely to occur. (Refer to Fig. 1)
The following documents also contain related information.