This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
A decoupling capacitor is recommended for stable circuit operation. The reason is that if AC components such as noise are superimposed on the power supply voltage supplied to the general purpose logic IC, it may cause voltage fluctuations and destabilize circuit operation.
By connecting the decoupling capacitor as close to the IC pin as possible, a stable power supply voltage with little noise can be supplied to the IC. The spiking current generated during switching causes the potential of VCC, GND to fluctuate, causing ringing of the output-waveform and speed delay. Therefore, the impedance of the power supply line against high frequency should be kept low.
Specifically, VCC and GND lines should be thick and short, and it is ideal to insert a decoupling capacitor (0.01 µF to 0.1 µF) close to the power pin of each IC, which acts as a high-frequency filter. Place the decoupling capacitor as close to each IC as possible. The distant placement not only reduces the effect, but may also radiate the switching noise of the IC.
For low-frequency filtering, a 10-µF to 100-µF capacitor is generally used for each board.
(Fig. 1)
The following documents also contain related information.