What is the slew rate control function of eFuse IC (electronic fuses) intended to do? And how does it works?

The slew rate control function is a feature that controls the slew rate of the output voltage to suppress inrush current.

When the output is turned on, an inrush current flows to charge the capacitor connected to the load side. If this current is too large, the overcurrent protection circuit may malfunction, making it impossible to start up, or overshooting may occur in the output voltage.
To prevent this, this function limits the inrush current and controls the slew rate at the rise of the output voltage.

Operational Waveform Image Without Slew Rate Control
Figure 1: Operational Waveform Image Without Slew Rate Control
Operational Waveform Image With Slew Rate Control
Figure 2: Operational Waveform Image With Slew Rate Control

Related Links

Please refer to the following pages and documents for product lineup and other documents.

자주 있는 문의

애플리케이션 노트

* Company names, product names, and service names used in this FAQ may be of their respective companies.

A new window will open