What applications are eFuse IC (electronic fuses) used for?

Toshiba eFuse IC can be used as power line protection ICs for such consumer electronics and industrial devices as shown below.

Typical uses are short-circuit protection of USB terminals and protection of subsequent ICs.
It is also suitable for protecting applications that require the safety standard IEC 62368-1.

Applications for Notebook PC/ Mobiles
Figure 1 Applications for Notebook PC/ Mobiles
Applications to Servers
Figure 2 Applications to Servers
Application to wearable/IoT
Figure 3 Application to wearable/IoT

Other applications

  • Printer
  • VR/AR
  • Smart Speakers
  • USB devices, etc.

Related Links

Please refer to the following pages and documents for product lineup and other documents.

자주 있는 문의

애플리케이션 노트

* Company names, product names, and service names used in this FAQ may be of their respective companies.

A new window will open