What is the under voltage lockout (UVLO) function of eFuse IC (electronic fuses) intended to do? And how does it works?

The undervoltage lockout (UVLO) function is a feature that turns off the output of the eFuse IC when the input voltage (VIN) falls below the set voltage value, preventing the subsequent circuit from malfunctioning.

If the input-voltage VIN drops, the subsequent circuitry may malfunction. Therefore, when VIN of eFuse IC falls below the UVLO voltage, the output of eFuse IC turns off to prevent the subsequent circuitry from malfunctioning. The operating voltage of UVLO is set internally in the IC. In addition, hysteresis is set in UVLO to prevent chattering, etc.
However, TCKE8 series can be adjusted by connecting two resistors.

Figure 1. Low-voltage malfunction prevention function (TCKE800/ 805/ 812 examples)
Figure 1. Low-voltage malfunction prevention function (TCKE800/ 805/ 812 examples)

Related Links

Please refer to the following pages and documents for product lineup and other documents.

자주 있는 문의

애플리케이션 노트

* Company names, product names, and service names used in this FAQ may be of their respective companies.

A new window will open