This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
If the input-voltage VIN drops, the subsequent circuitry may malfunction. Therefore, when VIN of eFuse IC falls below the UVLO voltage, the output of eFuse IC turnes off to prevent the subsequent circuitry from malfunctioning. The operating voltage of UVLO is set internally in the IC. In addition, hysteresis is set in UVLO to prevent chattering, etc.
However, TCKE8 series can be adjusted by connecting two resistors.