How can I achieve level shifting from 3.3V to 0.8V and vice versa?

Voltage conversion from step-down (3.3V → 0.8V) to step-up (0.8V → 3.3V) can be achieved using a level shifter (dual-supply type) capable of operating from 0.8V.

The following is a brief example.
For detailed selection methods, please use the following application notes.
Tips for Selecting Level Shifters(Voltage Translation ICs) (PDF:2.62MB)

Fig.1 Voltage Conversion (Step-Down) Using a Dual-Power-Supply Level Shifter
Fig.1 Voltage Conversion (Step-Down) Using a Dual-Power-Supply Level Shifter

Step-down voltage conversion:
3.3V → 0.8V and other high-to-low voltage conversions can be achieved on the input side using input tolerance functionality. To meet the operating voltage requirement of 0.8V output on the low-voltage side, devices capable of operating at 0.8V must be used. Using a device that outputs more than 0.8V on the low-voltage side could potentially damage the 0.8V device. Toshiba recommends using level shifters (dual-supply type) guaranteed to operate from 0.8V. (Fig.1, Table-1)

Table-1 Dual-Supply Level Shifter Capable of Operation from 0.8V
Product Name Operating Voltage Range Number of bit Direction
74AVC1T45 0.8V to 3.6V 1 Bidirectional
74AVCH1T45 0.8V to 3.6V 1 Bidirectional
74AVC2T45 0.8V to 3.6V 2 Bidirectional
74AVCH2T45 0.8V to 3.6V 2 Bidirectional
74AVC4T245 0.7V to 3.6V 4 Bidirectional
74AVCH4T245 0.7V to 3.6V 4 Bidirectional
74AVC4T345 0.7V to 3.6V 4 Bidirectional
Fig.2 Voltage Conversion Using a Dual-Power-Supply Level Shifter.
Fig.2 Voltage Conversion Using a Dual-Power-Supply Level Shifter.

Step-up voltage translation:
For voltage conversion from low voltages such as 0.8V to high voltages like 3.3V, the CMOS output of the preceding IC drives the CMOS input of the subsequent stage. Therefore, the high-level output voltage VOH ≈ the power supply voltage VCC. Voltage conversion is possible if the preceding stage's VOH satisfies the high-level input voltage VIH specification of the subsequent stage IC. Toshiba recommends using a level shifter (dual-supply type) as a product that satisfies the 0.8V VOH requirement. (Fig.2、Table.1)

Related Links

The following documents also contain related information.

FAQs

Product Lists

Application Notes