What happens after the overcurrent protection of the eFuse IC is activated and the IC is turned off?

Our eFuse ICs offer two options for recovery from overcurrent conditions: auto retry type and latched type.

The users can select the appropriate one from the two options depending on system requirements. The following two figures are timing charts showing the auto retry type and latch type of the TCKE8 series as examples. For further details, please refer to the datasheet.

Auto-Retry Type
Limits the current that flows through eFuse IC to the inside MOSFET by ILIM when the current exceeds the overcurrent limit ILIM. At this time, eFuse IC occurs power loss PD= (VIN - VOUT)×ILIM and the junction temperature rises, thus moves to thermal shutdown operation and turns off MOSFET.
After MOSFET turns off, junction temperature become lowers, then MOSFET turns on again. If the overcurrent condition is not resolved, ILIM limits the current and then performs the thermal shutdown operation again. (Figure 1)

Latch Type
Like the auto-retry type, after limiting the current flowing through MOSFET when an overcurrent occurs with the current determined by ILIM, eFuse IC moves to thermal shutdown and turns off MOSFET. The latch type keeps MOSFET off.
To release the latch state, after the overcurrent state is resolved, set the voltage of the EN / UVLO pin to the “L” level and then set it to the “H” level again. (Figure 2)

Timing Chart of Overcurrent Protection Operation (Auto-Retry Type)
Figure 1: Timing Chart of Overcurrent Protection Operation (Auto-Retry Type)
Timing Chart of Overcurrent Protection Operation (Latch Type)
Figure 2: Timing Chart of Overcurrent Protection Operation (Latch Type)

Related Links

Please refer to the following pages and documents for product lineup and other documents.

자주 있는 문의

애플리케이션 노트

* Company names, product names, and service names used in this FAQ may be of their respective companies.

A new window will open