This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
The Absolute Maximum Ratings that, in order to maintain an IC's life and reliability, must not be exceeded even for a moment. On the other hand, the operating range is a condition for guaranteeing normal operation, and this condition must be surely observed for use.
If any one of the operating ranges is exceeded, the IC operation cannot be guaranteed. Be sure to use ICs within the respective operating ranges. If it is difficult to do so, select other ICs with appropriate operating ranges.
The following documents also contain related information.