This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
A surge is a sudden rise in voltage that might damage electronic equipment.
Generally, voltage surges are classified into electrostatic discharge (ESD) and non-ESD surges. Non-ESD surges are caused by lightning strikes, the on/off of a switch, and power interruptions. As shown in Fig. 1, they last longer than ESD (for a period of milliseconds) and induce large energy. Although the transient overvoltage on transmission lines is also a type of surge, it is not covered herein. Non-ESD surges include direct lightning surges, induced lightning surges, and switching surges. It is rare to receive a direct lightning surge, but compared to other surges, the energy is large, and it is difficult to avoid destruction even if countermeasures are taken with electronic devices.
Direct lightning surges
As the name implies, a direct lightning surge occurs when lightning strikes a building, and lightning currents flow to the ground via electronic devices. A direct lightning strike has a current of several tens to several hundreds of kiloamperes, which is high enough to destroy all electronic equipment along the path of the lightning current. To prevent the destruction of electronic equipment, it is important to install a lightning protection device on a building.
Induced lightning surges
Induced lightning surges are caused by electromagnetic induction and electrostatic induction.
In addition to these, when a lightning strike causes the ground potential to rise, surge current might flow through a cable connecting between nearby and remote equipment. In this way, it is also necessary to protect against lightning surges other than direct lightning surges.
Switching surges
A switching surge is a sudden rise in voltage that occurs when a power line is opened and closed. A voltage surge (opening surge) occurs when a power line is turned on whereas a current surge (closing surge) occurs when it is cut off. The following describes the phenomena that occur in electronic circuits. Phenomena concerning utility grids are omitted here.
If no measures are taken, these
switching surges damage or degrade electronic equipment. These voltage and
current surges might be greater than the ESD voltage and current and therefore
can be a problem even for ESD-protected electronic equipment. Induced lightning
surges might occur when electronic equipment is connected to long wires such as
power lines and Ethernet cables. Switching surges might occur when electronic
equipment is connected to PLCs, long HVDC cables, or inductive loads such as
motors and relays.
Toshiba provides surge protection devices compliant with IEC 61000-4-5.
For products, please refer to the following links.