Tail Chain Control by NVIC

Timing improvement of exception/interrupt operation processing
Arm® Cortex®-M3 has become high-speed PUSH/POP processing through control of the NVIC.
In addition, if the interrupt request occurs at the same time or a high-priority interrupt request occurs during interrupt processing, the automatic save of registers by PUSH/POP is omitted, and the processing timing is improved.

Tail Chain Control by NVIC
Tail Chain Control by NVIC
Tail Chain Control by NVIC

第2章 Arm® Cortex®-M3

Hardware Configuration
NVIC (Nested Vectored Interrupt Controller)
Main Core
Register Configuration
The Role of the Register
Stack Pointer
PUSH/POP to the Stack Pointer
Special Register
Operation Mode and Stack Pointer (1)
Operation Mode and Stack Pointer (2)
Exceptions (Reset, Interrupt, Fault, System Call)
The Role of NVIC
Memory Map
Memory Map for Arm® Cortex®-M3 Specifications
Memory Map of TMPM330: Example of TX03 Series
Vector Table (1)
Vector Table (2)
Bit Band Area and Bit Band Alias Area (1)
Bit Band Area and Bit Band Alias Area (2)

* Arm and Cortex are registered trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere.

A new window will open