When a spike-voltage is applied to the input or output terminals of eFuse IC (electronic fuse), How do I take measures?

It is possible to take countermeasures by using a Zener diode or SBD (Schottky Barrier Diode).

If the transient voltage at the input terminal of the eFuse IC exceeds the absolute maximum rating, connect a Zener diode between the input terminal and GND.
For negative spike voltage generated on the output side, SBD (Schottky barrier diode) can be connected to prevent the output potential from dropping below GND.
To reduce the inductance of the pattern connected to the eFuse IC, make the length on the input and output sides as short as possible, and make the GND area as wide as possible to reduce the impedance.

Figure 1. Typical eFuse IC Spike-Voltage Protection Diodes
Figure 1. Typical eFuse IC Spike-Voltage Protection Diodes

Related Links

Please refer to the following pages and documents for product lineup and other documents.

자주 있는 문의

애플리케이션 노트

* Company names, product names, and service names used in this FAQ may be of their respective companies.

A new window will open