This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
It is possible to take countermeasures by using a Zener diode or SBD (Schottky Barrier Diode).
If the transient voltage at the input terminal of the eFuse IC exceeds the absolute maximum rating, connect a Zener diode between the input terminal and GND.
For negative spike voltage generated on the output side, SBD (Schottky barrier diode) can be connected to prevent the output potential from dropping below GND.
To reduce the inductance of the pattern connected to the eFuse IC, make the length on the input and output sides as short as possible, and make the GND area as wide as possible to reduce the impedance.
Please refer to the following pages and documents for product lineup and other documents.
* Company names, product names, and service names used in this FAQ may be of their respective companies.