What is the rapid output discharge function of the TCKE9 series?

In the TCKE9 series, there are "TCKE903QNA" and "TCKE905QNA" equipped with a "rapid output discharge function."

In the "TCKE9xxQNA," a discharge MOSFET is built into the IC, and a "rapid output discharge function" is provided that quickly discharges the charge stored in the capacitor connected to the VOUT terminal when the output is OFF. This function is enabled by connecting the QOD terminal and the VOUT terminal directly or via an external resistor (see Figure 1). If the QOD terminal is OPEN, the output discharge time is determined by the output capacitor and the load. Figures 2 and 3 show examples of discharge waveforms for the TCKE9xxQNA.
On the other hand, products other than the TCKE9xxQNA do not have a discharge MOSFET built into the IC, and output discharge is performed through the internal circuit. Therefore, it is not designed for active output discharge, and compared to the TCKE9xxQNA, the discharge speed is slower.

Example of a rapid output discharge circuit using TCKE9xxQNA
Figure 1. Example of a rapid output discharge circuit using TCKE9xxQNA

RQODEXT = OPEN
VIN = 5.0V, EN = H to L, COUT = 100μF, ROUT = 1kΩ, Ta = 25ºC

RQODEXT = OPEN VIN = 5.0 V, EN = H to L, COUT = 100 μF, ROUT = 1 kΩ, Ta = 25 ºC

RQODEXT = Short
VIN = 5.0V, EN = H to L, COUT = 100μF, ROUT = 1kΩ, Ta = 25 ºC

RQODEXT = Short VIN = 5.0 V, EN = H to L, COUT = 100 μF, ROUT = 1 kΩ, Ta = 25 ºC

Figure 2. Discharge waveform of TCKE905QNA

RQODEXT = OPEN
VIN = 3.3V, EN = H to L, COUT = 100μF, ROUT = 1kΩ, Ta = 25 ºC

RQODEXT = OPEN VIN = 3.3 V, EN = H to L, COUT = 100 μF, ROUT = 1 kΩ, Ta = 25 ºC

RQODEXT = Short
VIN = 3.3V, EN = H to L, COUT = 100μF, ROUT = 1kΩ, Ta = 25 ºC

RQODEXT = Short VIN = 3.3 V, EN = H to L, COUT = 100 μF, ROUT = 1 kΩ, Ta = 25 ºC

Figure 3. Discharge waveform of TCKE903QNA

Related Links

Please refer to the following pages and documents for product lineup and other documents.

자주 있는 문의

애플리케이션 노트

* Company names, product names, and service names used in this FAQ may be of their respective companies.

A new window will open