This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
In the TCKE9 series, there are "TCKE903QNA" and "TCKE905QNA" equipped with a "rapid output discharge function."
In the "TCKE9xxQNA," a discharge MOSFET is built into the IC, and a "rapid output discharge function" is provided that quickly discharges the charge stored in the capacitor connected to the VOUT terminal when the output is OFF. This function is enabled by connecting the QOD terminal and the VOUT terminal directly or via an external resistor (see Figure 1). If the QOD terminal is OPEN, the output discharge time is determined by the output capacitor and the load. Figures 2 and 3 show examples of discharge waveforms for the TCKE9xxQNA.
On the other hand, products other than the TCKE9xxQNA do not have a discharge MOSFET built into the IC, and output discharge is performed through the internal circuit. Therefore, it is not designed for active output discharge, and compared to the TCKE9xxQNA, the discharge speed is slower.
RQODEXT = OPEN
VIN = 5.0V, EN = H to L, COUT = 100μF, ROUT = 1kΩ, Ta = 25ºC
RQODEXT = Short
VIN = 5.0V, EN = H to L, COUT = 100μF, ROUT = 1kΩ, Ta = 25 ºC
Figure 2. Discharge waveform of TCKE905QNA
RQODEXT = OPEN
VIN = 3.3V, EN = H to L, COUT = 100μF, ROUT = 1kΩ, Ta = 25 ºC
RQODEXT = Short
VIN = 3.3V, EN = H to L, COUT = 100μF, ROUT = 1kΩ, Ta = 25 ºC
Figure 3. Discharge waveform of TCKE903QNA
Please refer to the following pages and documents for product lineup and other documents.
* Company names, product names, and service names used in this FAQ may be of their respective companies.