This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Microcontrollers use various combinations of the logic circuits explained so far.
In the logic circuits introduced so far, if the input changes, the output changes at the same time. Its data cannot be stored.
On the other hand, a circuit that stores the information given in the past is called a sequential circuit (Feedback circuit).
The flip-flop circuit is the prototype of the storage circuit that is closely related to the microcontroller.
The word ”flip-flop” originally means "pitter-patter sound" or "the state changes suddenly".
Another name is also called a bi-stable multi vibrator.
As the name implies, it has two stable states. It is set by the input condition that determines one state.
This state is retained or stored until an input condition that determines the other states are given.
Flip-flops have RS, T, D, JK, etc., depending on how 0 and 1 are stored.