This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
By combining the basic logic circuits described so far, a circuit with a specific function can be configured.
Here, we will explain about the XOR (*) circuit used for a comparator that checks for the data mismatch and the adder.
The switch in the figure defines the pressed state as "ON" and the pulled state as "OFF".
When switch A is "ON", the upper circuit is connected and the lower circuit is disconnected.
On the contrary, when it is "OFF", the lower circuit is connected and the upper circuit is disconnected.
When switch B is "ON", the upper circuit is disconnected and the lower circuit is connected.
On the contrary, when it is "OFF", the lower circuit is disconnected and the upper circuit is connected.
If the A and B switches are combined as shown in the figure, no current will flow and the light bulb will not turn on, when both A and B are "ON" or both are "OFF".
The circuit is connected and the light bulb is turned on only when A and B do not match, such as A is “ON” and B is “OFF”.
As shown in the truth table, the output Y is 1 when 1 is input to either of A and B.
The schematic can be expressed by the MIL symbol as shown in the right figure.
* Abbreviation for Exclusive OR