This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Here, we introduce how to easily convert the decimal number to the binary number and the hexadecimal number.
To represent the decimal number 100 as a binary number, firstly divide 100 by 2.
It is divisible by 50 and the remainder is 0.
Next, divide 50 by 2 to get 25, divide 25 by 2, remove 1 of the remainder at this time, and continue the calculation until it is not divided by an integer.
When the remainder of the calculation results are collected in order from the bottom to the top, it is converted to the binary number.
When the decimal number 100 is converted to a binary number, it becomes (1100100).
So what about the hexadecimal number?
If 100 is divided by 16, it is 6 with a remainder of 4.
Therefore, when the decimal number 100 is converted to the hexadecimal number, it becomes 64.