This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
The OR circuit is called the logical disjunction circuit.
The OR circuit can be thought of as a circuit that outputs when either signal is input.
In same as on the previous page, let's consider an example of turning on a light bulb.
The AND circuit was connected in series, but this OR circuit is connected in parallel.
In other words, if either A or B is ON, the light bulb will be ON.
As shown in the truth table, the output Y will be 1 if 1 is input to either A or B.
The schematic can be expressed by the MIL symbol as shown in the right figure.