This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
The AND circuit is also called the logical conjunction circuit.
The AND logic can be thought of as a circuit that outputs an output signal when all input conditions are satisfied.
For example, when you want to turn on the light bulb, even if switch A is ON, the light bulb does not turn on if switch B is OFF.
On the contrary, even if switch B is ON, the light bulb still does not turn on if switch A is OFF.
So this means that the light bulb will only turn on when both switches A and B are ON.
As shown in the truth table, output Y is 1 only if 1 is input to both A and B.
The circuit diagram can be expressed by the MIL symbol (*) as shown in the right figure.
* A symbol used in the digital circuit diagram defined by the US military standard "MIL Standard".
MIL Standard (Military Standard): Military supplies procurement standard standardized by the US Department of Defense