What is the difference between TVS diode and Zener diode for protection?

Both are diodes designed to protect circuits from electrostatic discharge (ESD) and overvoltage surges, but the types of surges they handle, and their applications differ.

The coverage areas of TVS diodes and protection Zener diodes

Our lineup of TVS (Transient Voltage Suppressor) diodes and protection Zener diodes are semiconductor devices that utilize the reverse characteristics of diodes and have the following features.

  • TVS Diode
    Primarily protects circuits from ESD, switching surges, and other transient overvoltage events. Under normal conditions, they remain in a non-conductive standby state. When an abnormal overvoltage surge occurs, they respond at nanosecond-level speed to clamp the voltage and protect the circuit. TVS diodes are mainly used for communication lines and power lines, but products with low terminal capacitance are also available, making them suitable for high-speed communication line protection.
  • Protection Zener Diode
    Similarly, these diodes protect circuits from transient overvoltage surges such as ESD and switching surges. However, they can also handle surges that are close to DC, which TVS diodes cannot effectively address. They are mainly used for protecting power line sections.

Such protection devices are widely used to safeguard communication lines and power lines in consumer, industrial, and automotive equipment.
The following summarizes the coverage areas of TVS diodes and protection Zener diodes for your reference.

  ESD protection (TVS) diode Protection Zener diode
Main applications Protection against overvoltage surges of microsecond order or less*1 Protection against overvoltage surges longer than microseconds (Can also be used for ESD protection *1)
Terminal-to-terminal capacitance*2 0.12pF to 600pF 100pF to 600pF
Examples of usage locations USB, HDMI connectors, power lines etc. Power lines, power control lines
Remarks Lineup mainly consists of products with low capacitance of 1pF or less. If within allowable loss, protection is possible even from overvoltage pulses close to DC.

*1 Applicable standards: IEC61000-4-2, IEC61000-4-5 (8/20μs conditions)
*2 For details, please refer to the individual data sheets

Related Links

There are related explanations in the following materials, so please refer to them.

FAQs

Application Notes

* Company names, product names, and service names used in this FAQ may be of their respective companies.

A new window will open