This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Both are diodes designed to protect circuits from electrostatic discharge (ESD) and overvoltage surges, but the types of surges they handle, and their applications differ.
Our lineup of TVS (Transient Voltage Suppressor) diodes and protection Zener diodes are semiconductor devices that utilize the reverse characteristics of diodes and have the following features.
Such protection devices are widely used to safeguard communication lines and power lines in consumer, industrial, and automotive equipment.
The following summarizes the coverage areas of TVS diodes and protection Zener diodes for your reference.
| ESD protection (TVS) diode | Protection Zener diode | |
|---|---|---|
| Main applications | Protection against overvoltage surges of microsecond order or less*1 | Protection against overvoltage surges longer than microseconds (Can also be used for ESD protection *1) |
| Terminal-to-terminal capacitance*2 | 0.12pF to 600pF | 100pF to 600pF |
| Examples of usage locations | USB, HDMI connectors, power lines etc. | Power lines, power control lines |
| Remarks | Lineup mainly consists of products with low capacitance of 1pF or less. | If within allowable loss, protection is possible even from overvoltage pulses close to DC. |
*1 Applicable standards: IEC61000-4-2, IEC61000-4-5 (8/20μs conditions)
*2 For details, please refer to the individual data sheets
There are related explanations in the following materials, so please refer to them.
* Company names, product names, and service names used in this FAQ may be of their respective companies.