Contact us

A new window will open A new window will open

Do semiconductor devices tolerate the rated absolute maximum conditions if such conditions exist only instantaneously?

The absolute maximum ratings of a semiconductor device are a set of ratings that must not be exceeded, even for a moment. Do not exceed any of these ratings. Exceeding the rating(s) may cause the device breakdown, damage or deterioration, and may result injury by explosion or combustion. Therefore, the rated absolute maximum conditions must not be exceeded under any circumstances.
For details, see the Reliability Information page.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.