Contact us

A new window will open A new window will open

A dotted line in a safe operating area is annotated as “This area is limited by RDS(ON).” What does it mean?

This line represents an area bound by a conduction loss that occurs while the MOSFET is on. Because of its electrical characteristics, the MOSFET cannot operate in an area above the line limited by RDS(ON).



It is represented by the straight line shown in ② in the figure.
This straight line is calculated by the expression ID = VDS / RDS (ON) max.

Maximum Ratings: Power MOSFET Application Notes (PDF:1,075KB)
https://toshiba.semicon-storage.com/info/docget.jsp?did=13414

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.