1-2-2. Logic Circuit: OR Circuit

OR circuit
OR circuit

The OR circuit is called the logical disjunction circuit.
The OR circuit can be thought of as a circuit that outputs when either signal is input.

In same as on the previous page, let's consider an example of turning on a light bulb.
The AND circuit was connected in series, but this OR circuit is connected in parallel.
In other words, if either A or B is ON, the light bulb will be ON.

As shown in the truth table, the output Y will be 1 if 1 is input to either A or B.
The schematic can be expressed by the MIL symbol as shown in the right figure.

Chapter 1 Basics of Digital Circuits

1-1. Digital Value
1-1-1. Digital Value: Binary and Decimal
1-1-2. Digital Value: Units of Binary Data
1-1-3. Digital Value: Notation Method of Data
1-1-4. Digital Value: Conversion Method of the Data
1-2. Logic Circuit
1-2-1. Logic Circuit: AND Circuit
1-2-3. Logic Circuit: NOT Circuit
1-2-4. Logic Circuit: Exclusive OR (XOR) Circuit
1-2-5. Logic Circuit: 3 State Buffer (1)
1-2-6. Logic Circuit: 3 State Buffer (2)
1-2-7. Logic Circuit: Application Example of Logic Circuits
1-2-8. Logic Circuit: RS flip-flop Circuit
A new window will open