Contact us

A new window will open A new window will open

If the packages are the same, are the thermal resistances the same?

Even if the packages are the same, the thermal resistances are not always the same.
Thermal resistance varies depending on chip size and internal structure, too.

If the package is the same but the thermal resistance is different, even if the same power dissipation occurs, the junction temperature of the semiconductor device is different.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.