Contact us

A new window will open A new window will open

What is a radiation equivalent circuit?

A radiation equivalent circuit (Figure 1) is a thermal circuit described by an electrical circuit.
By replacing the heat flow by current, the heat path conducted to the outside can be represented by an electric circuit.
Figure 2 shows the thermal resistance from device junction to ambient.



For radiation equivalent circuit, please refer to “Thermal Design and Attachment of a Thermal Fin: Power MOSFET Application Notes (PDF:1,061KB)

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.