Contact us

A new window will open A new window will open

What does derating of Safe Operating Area (SOA) mean?

Derating of SOA is to calculate the SOA based on the ambient temperature (or case temperature) of semiconductor device in operation.
The SOA in the datasheet is specified at 25 [deg.C] (ambient temperature or case temperature).
When the ambient temperature (or case temperature) is higher than 25 [deg.C], the SOA becomes narrow.
SOA should be limited by allowable power dissipation (within the junction temperature at the absolute maximum rating) based on ambient temperature.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.