1-2-1. Logic Circuit: AND Circuit

AND circuit
AND circuit

The AND circuit is also called the logical conjunction circuit.
The AND logic can be thought of as a circuit that outputs an output signal when all input conditions are satisfied.

For example, when you want to turn on the light bulb, even if switch A is ON, the light bulb does not turn on if switch B is OFF.
On the contrary, even if switch B is ON, the light bulb still does not turn on if switch A is OFF.
So this means that the light bulb will only turn on when both switches A and B are ON.
As shown in the truth table, output Y is 1 only if 1 is input to both A and B.
The circuit diagram can be expressed by the MIL symbol (*) as shown in the right figure.

* A symbol used in the digital circuit diagram defined by the US military standard "MIL Standard".
MIL Standard (Military Standard): Military supplies procurement standard standardized by the US Department of Defense

Chapter 1 Basics of Digital Circuits

1-1. Digital Value
1-1-1. Digital Value: Binary and Decimal
1-1-2. Digital Value: Units of Binary Data
1-1-3. Digital Value: Notation Method of Data
1-1-4. Digital Value: Conversion Method of the Data
1-2. Logic Circuit
1-2-2. Logic Circuit: OR Circuit
1-2-3. Logic Circuit: NOT Circuit
1-2-4. Logic Circuit: Exclusive OR (XOR) Circuit
1-2-5. Logic Circuit: 3 State Buffer (1)
1-2-6. Logic Circuit: 3 State Buffer (2)
1-2-7. Logic Circuit: Application Example of Logic Circuits
1-2-8. Logic Circuit: RS flip-flop Circuit
A new window will open