Contact us

A new window will open A new window will open

Technical documents for individual power transistors contain a safe operating area (SOA) graph. What is it?

The safe operating area (SOA) is very important for the operation of a power transistor because the SOA graph specifies the voltage and current conditions in which a power transistor can be used safely. The borders of the safe operating area are broadly defined by a thermal dissipation limit and the limit given by secondary breakdown.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.