This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Interrupts have two types: Hardware interrupt and Software interrupt.
The hardware interrupt occurrs by the interrupt request signal from peripheral circuits.
On the other hand, the software interrupt occurrs by executing a dedicated instruction.
The hardware interrupt has an external interrupt and an internal interrupt.
The external interrupt occurs when a specified signal is input to the dedicated external interrupt terminal.
The internal interrupt occurs by an interrupt request signal from a peripheral circuit built into the microcontroller.
In addition, it has a maskable interrupt and a non maskable interrupt depending on how the interrupt request signal is received.