This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Figure (a) shows the schematic of a voltage-resonant induction cooktop as an application example of soft switching. Figure (b) shows its operation and waveforms.
In the circuit of Figure (a), when the IGBT turns on, current flows through the heating coil (L1). When the IGBT turns off, L1 and C1 go into resonance, causing sinusoidal voltage to be applied to the IGBT. The direction of resonance between L1 and C1 reverses, causing the C1 voltage to offset the C2 voltage. When the C1 voltage exceeds the C2 voltage, current begins to flow through the C1-C2-FWD-C1 loop. During this period, the collector-emitter voltage of the IGBT is equal to the forward voltage (VF) of the freewheeling diode (FWD), which is almost zero. At this time, the IGBT turns back on. As a result, current flows through the heating coil (L1) from the input side again. This sequence is repeated.
A voltage-resonant circuit is inexpensive because it does not require many components. However, when a system needs a high power capacity, an IGBT with very high withstand voltage is required so as to handle high resonance voltage. Therefore, a voltage-resonant circuit is used in many induction home appliances with a capacity of up to 1.5 kW at 100 VAC and up to 3 kW at 200 VAC. The smoothing capacitor (C2) on the input side has low capacitance because it receives electric power during a single pulse period. The voltage across C2 has a full-sine waveform, leading to a high power factor on the input side. Therefore, a voltage-resonant circuit eliminates the need for a power factor correction (PFC) circuit.
Steps 1 to 3 are repeated.