This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Triac couplers are a kind of photocoupler used as a trigger mainly for the main triac. SSR (solid state relays) is a semiconductor relay consisting of a triac coupler, main triac, resistance, and capacitor. Triac couplers alone can turn a load ON/OFF. However, the current they can control is so small (around 100mA) that SSR is used for applications for performing ON/OFF control on large currents. Owing to their structure, triac couplers have a tendency to hold a current flowing through the triac once they are turned ON. Even if LED signals are turned OFF after that, the triac couplers will not turn OFF unless the current flowing through the triac becomes a certain current (holding current) level or smaller. For that reason, triac couplers cannot perform OFF control in conjunction with LED signals. Photorelays are also a kind of semiconductor relay. They have a tendency to be able to control both ON and OFF operations in conjunction with LED signals.