Contact us

A new window will open A new window will open

If multiple outputs from a general-purpose CMOS logic IC come into conflict, is the IC adversely affected?

An IC with 3-state outputs could be deteriorated if it is used for a long time with multiple outputs enabled.

[Figure: Output conflict in a device with 3-state outputs]

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.