Contact us

A new window will open A new window will open

Why are two MOSFETs used in series in the Lithium-ion secondary battery protection circuit?

充放電機能を実現するために、このように2個のMOSFETを使用しております。

In order to achieve the charge-discharge function, two MOSFETs are used as shown in Figure 1.

The case of only one MOSFET is used as shown in Figure 2, even if the MOSFET is turned off, reverse current of MOSFET flow through the body diode in discharge of Lithium-ion secondary battery.
This case will not be a function as a charge-discharge switch.

MOSFETを1個だけ使用した場合、充放電スイッチとしては機能しません。

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.