This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Select products with short inverse recovery time trr, low peak reverse recovery current Irr, and low forward voltage VF.
Due to the circuit operation of the bridging circuit, there is a mode in which Q2 is turned on while a return current is flowing to Q1 diode. (Fig. 1-①).
At this time, Q1 diode enters the reverse-recovery operation, but during this time, Q1 and Q2 are short-circuited (Fig. 1-②), causing a large drop (Fig. 1).
The reverse recovery time of body diodes tends to be longer for high-voltage products than for low-voltage products, but we offer a lineup of high-speed diodes with a shorter reverse recovery time for high-voltage products.
Please select the product group with the suffix "5" (e.g. TK16A60W5).
Please confirm the product lineup.