This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Two MOSFET are used to realize both the charge and discharge functions.
To realize both the charge and discharge functions, two MOSFET are used as shown in Fig. 1.
The case of only one MOSFET is used as shown in Fig. 2., even if the MOSFET is turned off, reverse current of MOSFET flow through the body diode in discharge of Lithium-ion secondary battery.
This case will not be a function as a charge-discharge switch.
Please also refer to the following page.