2-6. Classification by Stator

Classification by stator

Stepping motors are also classified by the number of stators.
If there are two stators, it is called "2-phase motor", if there are three stators, it is called "3-phase motor", and if there are five stators, it is called "5-phase motor".

Chapter 2 Features and Classifications of Stepping Motors

2-1. Open-Loop Control
2-2. Pros and Cons
2-3. Classification by Output Power
2-4. Classification by Power Supply
2-5. Unipolar Type and Bipolar Type
2-7. Classification by Rotor Types
A new window will open