This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Even TVS diodes with high ESD protection performance do not provide sufficient ESD protection without adequate board design. In particular, board design affects the instantaneous high-frequency pulse that occurs upon ESD entry.
The following figure compares the clamp voltage waveforms, depending on the distance of a TVS diode from a connector, and the ESD entry point. As can be seen from this figure, when a TVS diode is placed close to the connector (i.e., far from the IC under protection), the first peak voltage (i.e., the voltage immediately after ESD entry) is nearly 10 V lower than the case in which it is placed close to the IC.
The following considerations apply to board design: