This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Increasing the capacitance of the output capacitor COUT is effective in improving the load transient response of an LDO.
During a sudden load current change, the output voltage variation (∆VOUT) and the output capacitor (COUT) can be expressed as follows.
Therefore, increasing the capacitance of COUT reduces the output voltage variation ∆VOUT, resulting in improved load transient response.
However, increasing the capacitance could cause inrush current, and oscillation. In addition, it is important to pay attention to the VOUT startup characteristics.
For more details, please refer to the application note titled
“Load Transient Response of LDO and Methods to Improve it”
COUT : Output capacitor
∆VOUT : Output voltage variation
∆IOUT : Output current variation
T : the duration during which current flows
Note:
The following documents also contain related information.