This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
An op-amp is an IC that amplifies the difference in voltage between two inputs. The desired circuit can be easily designed with a few external resistors. Also, when common-mode noise becomes a problem in noisy environments, the differential input of the op-amp can reject it. For this reason, it is often used in various sensors that are often used in IoT Devices, etc.
In the most basic circuit, op-amps are used as voltage amplifiers, which can be broadly divided into noninverting and inverting amplifiers. Voltage followers (also simply called buffers) are a type of commonly used noninverting amplifiers. Op-amps are also used as differential amplifiers, integrator circuits, etc.
Op-amps are widely used for various applications. It is no exaggeration to say that op-amps are found in almost all electrical appliances. For example, op-amps amplify analog signals from various sensors in IoT-connected home appliances and measuring instruments.
The following documents also contain related information: