This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
When connecting a microcontroller with 16-bit data bus and a NOR Flash memory with 16-bit data bus, connect the address port pin A1 of the microcontroller to the address port pin A0 of the NOR Flash, A2 of the microcontroller to A1 of the NOR Flash and so on. (The address port pin A0 of the microcontroller is not used.) This is because although NOR Flash addresses are assigned on a byte-by-byte basis, only even addresses (address 0, address 2, address 4, etc.) are accessed.
Connection Example
The following shows an example of connection between the TMP92CF29A and a 16-bit NOR Flash memory.
Connection Example
The following shows an example of connection between the TMPM341FXBG and a 16-bit NOR Flash memory.
* Before making actual connection, be sure to check the datasheet of the microcontroller you are using for device-specific details.
(NO.EB9900401 2011/11/01)