This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Power dissipation is the maximum power that the MOSFET can dissipate continuously under the specified thermal conditions. It is defined between channel (ch) - case (c) or ch - ambient air (a) when mounting an infinite heat sink.
When a heat sink is attached to a MOSFET, power dissipation is calculated from the sum of 1) channel-to-case thermal resistance (internal thermal resistance), 2) insulator thermal resistance, 3) contact thermal resistance, and 4) heat sink thermal resistance. For MOSFETs housed in a surface-mount package, power dissipation is specified in the case of mounting on a board. The board size is specified in individual technical data sheets.
The allowable power dissipation varies with the conditions under which the MOSFET is used (such as ambient temperature and heat dissipation conditions). In practice, power dissipation should be calculated from channel-to-ambient thermal resistance in the end-use application environment.
Thermal Design and Attachment of a Thermal Fin: Power MOSFET Application Notes (PDF:1,061KB)
Maximum Ratings: Power MOSFET Application Notes (PDF:1,075KB)