This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The BRT contains resistors R1 and R2 as shown in Figure 2.*
The definition of the hFE of the BRT is different from that of typical bipolar transistors and is expressed by the following equations:
hFE = IC / IB = IC / ( Ib + IR2 ) ... (1)
IR2 = Vbe / R2 = 0.7** / R2 ... (2)
In the case of typical bipolar transistors or BRTs containing only R1, IB = Ib. Hence, hFE is expressed as:
hFE = IC / Ib ... (3)
The hFE of the BRT differs from that of typical bipolar transistors in that the denominator of Equation (1) includes IR2.
#1: Equation (2) indicates that IR2 is inversely proportional to R2. BRTs with a higher R2 value exhibit a higher hFE.
#2: Ib in the denominator is proportional to IC, but IR2 is a constant value dependent only on R2.
Therefore, hFE decreases in the low collector-current region because of a greater effect of R2.
Obviously, BRTs without R2 and typical bipolar transistors do not exhibit this characteristic.***
*: BRTs without R2 are also available.
**: Vbe changes with collector current (IC). However, since Vbe changes only slightly, it is assumed to be constant at 0.7 V.
***: In the lower collector-current region, hFE might decrease because of the effect of leakage current.