This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Neither junction-to-case thermal resistance, Rth(j-c), nor channel-to-case thermal resistance, Rth(ch-c), is specified for small-package devices.
This is because heat dissipation mainly occurs through the leads, and the package surface area is very small, making it difficult to accurately define and measure a representative case temperature.
For this reason, junction-to-case or channel-to-case thermal resistance is not an appropriate parameter for thermal evaluation of small-package devices.
For information on calculating junction or channel temperature, please refer to the following FAQ:
> How to calculate the junction temperature of a semiconductor device whose datasheets do not include a “thermal resistance” value